Skip to main content
Senior
September 14, 2025
Solved

What is the proper syntax for aligning a struct, and a member within that struct?

  • September 14, 2025
  • 4 replies
  • 1641 views

Hi,

I have a struct that looks like the following:

typedef struct {
 uint8_t statusbyte;
 uint8_t dmaBuffer[32];
} STRUCT_ReceptionBuffer;

The RM0091 instructs that source and destination addresses should be aligned on the data size. What I want to transfer to the buffer are 32-bit words (it is an I2S-to-USB-Audio conversion, and USB deals with bytes).

This means I need to align the struct. I am using the GCC compiler tools but the F0 HAL library also defines the __ALIGN_BEGIN and __ALIGN_END macros.

My question is, how and where should I place these macros in order for them to have the desired effect?

Does this look correct?

typedef __ALIGN_BEGIN struct {
 uint8_t statusByte;
 __ALIGN_BEGIN uint8_t dmaBuffer[32] __ALIGN_END;
} STRUCT_ReceptionBuffer __ALIGN_END;

Or would this be more correct?

 

typedef struct __ALIGN_BEGIN {
 uint8_t statusByte;
 __ALIGN_BEGIN uint8_t __ALIGN_END dmaBuffer[32];
} __ALIGN_END STRUCT_ReceptionBuffer ;

 

The complier does not seem to care much what I do. Even the following blatantly-wrong looking definition is completely fine?

typedef struct {
 uint8_t statusByte; __ALIGN_END
 uint8_t __ALIGN_END dmaBuffer[32];
} __ALIGN_END STRUCT_ReceptionBuffer;

Is this just a matter of trial and error? Or is it so that the compiler really doesn't care, and any errors caused by this only pop up during runtime?

Best answer by Pavel A.

@ankes Placement of __attribute__ sometimes is quirky. Newer gcc versions (and clang) warn about possibly wrong placement of  __attribute__ , so keep an eye on compiler warnings.

 

4 replies

Pavel A.
Super User
September 14, 2025

It's not clear what do you actually want: 

A. define a structure so that members are properly aligned

B. Unpack byte-packed data to C struct with properly aligned members

C. Define a tightly packed structure (prevent adding pad bytes between struct members)  though some struct members won't be aligned.

ankesAuthor
Senior
September 15, 2025

@Pavel A. I want to define a structure where the member "dmaBuffer" is 32-bit -aligned, to ensure that using DMA to transfer data to it is safe, regardless of where the beginning of the struct ("statusByte") resides.

This syntax seems to achieve what I want:

typedef struct {
 uint8_t statusByte;
 __ALIGN_BEGIN uint8_t dmaBuffer[32] __ALIGN_END;
} STRUCT_ReceptionBuffer;

Looking at the memory view, the first member of "dmaBuffer" resides at a 32-bit boundary (in my specific case, at 0x200009b4).

I also tested a scenario where I removed the __ALIGN_* macros. In the memory view, "dmaBuffer" moved to start from 0x200009b1, and the DMA transfer started writing over "statusByte" as well.

So, case closed. If you know the syntax how to align the struct itself, then that'd be appreciated. This latter is just for out of curiosity, not necessity.

gbm
Principal
September 14, 2025

Use standard C language feature - _Alignas keyword (in C23 - alignas).

Or - maybe more suitable in your case - declare the buffer as union:

union {
 uint32_t buf_as_words[8];
 uint8_t buf_as_bytes[32];
};
My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
ankesAuthor
Senior
September 15, 2025

@gbm Thank you for the suggestion.

Switching to "c23" would require me to modify the "usbd_desc.c" file, and change the __ALIGN_* macros that STM32CubeIDE generated for me, in order for things to be consistent.

I could do that, so I will take this possibility into consideration.

gbm
Principal
September 15, 2025

You need to align the data buffer being a member of a structure, not the structure as a whole. I suggested two standard ways of doing this without using strange non-standard macros. Since you need to access the buffer as bytes and as words, the union is the way to go, so that you don't need to do the type casts.

_Alignas(uint32_t) uint8_t dmaBufrer;

will work with C11 and above. C23 introduces all-lowercase alignas keyword. GCC13 supplied with CubeIDE supports C23.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Karl Yamashita
Principal
September 15, 2025

The structure is uint8_t throughout, so there is nothing to align.

You mentioned you need to transfer 32 bit values to the buffer. Did you mean to define the dmaBuffer as uint32_t and not uint8_t?  

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
TDK
Super User
September 15, 2025

This will work:

typedef struct {
 uint8_t statusbyte;
 uint8_t dmaBuffer[32] __attribute__((aligned(4)));
} STRUCT_ReceptionBuffer;

as will this:

typedef struct {
 uint8_t statusbyte;
 __attribute__((aligned(4))) uint8_t dmaBuffer[32];
} STRUCT_ReceptionBuffer;

 The structure itself will always be aligned since one of its members requires 4-bytes alignment. In other words, no need to do this:

__attribute__((aligned(4))) STRUCT_ReceptionBuffer rx;

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
gbm
Principal
September 16, 2025

@TDK wrote:

This will work

As will this, without non-C-standard __attribute__ and with less characters to type. ;)

typedef struct {
 uint8_t statusbyte;
 _Alignas(uint32_t) uint8_t dmaBuffer[32];
} STRUCT_ReceptionBuffer;

Another side remark - typedef should be avoided here, just for coding style clarity.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice