Working with SW4STM32 Workspaces, what are the RULES, why PROPERTIES won't show the present WORKSPACE?
I am new to STM32F products and SW4STM32 Development Tools including CubeMX. I also own a STM32F303RE Eval Brd. While working with SW4STM32 (IDE) I created a WORKSPACE; part of the initial opening. Also, the INITIAL install of STM32Cube_F3 included the locations of the PROJECT EXAMPLES. The first time I used SW4STM32, the tool opened and ask for a WORKSPACE. The tool actually picked the workspace and all I needed to do was accept. While working with the tools I noted the original EXAMPLES file got changed. I was working with EXAMPLES\GPIO\GPIO_IOToggle. I decided to back-track to see how the files got changed.
My thought was to go back and reload STM32Cube_F3 again in a new directory, thus restoring all the examples to their initial state. I wanted the changed EXAMPLE files in the initial STM32Cube_F3 to remain in the changed state. I then proceeded to open the GPIO EXAMPLE again under the new STM32CubeF3 install using the SW4STM32 (IDE). This did not work so well.
When I opened the SW4STM32 the PROJECT EXPLORER was empty. The design space was 100% empty. I went over to the PROJECT TAB and the OPEN PROJECT selection was grayed out. I then went to SWITCH WORKSPACE and that's when the problems began; the SW4STM32 would reboot in a loop, coming back to a same blank environment. I spent several minutes trying to load the EXAMPLES and there was no way to do it, not even through IMPORT. The IMPORT procedure stated there was a WORKSPACE issue.
I finally went back to SWITCH WORKSPACE and selected one of the two choices offered by the tool. I noted there were four previous projects in PROJECT EXPLORER; this was a relief, seemed I found a valid WORKSPACE.
I proceeded to IMPORT the GPIO_IOToggle example and the SW4 IDE TOOL would not let it load. The tool complained about WORKPLACE conflict.
I then opened MS WINDOWS EXPLORER where the GPIO_IOToggle was located, selected it, Dragged and Dropped the selected PROJECT file into SW4 PROJECT EXPLORER. The SW4 IDE took the GPIO PROJECT and loaded it into PROJECT EXPLORER window. I looked at MAIN.C properties and noted the file had a PATH RESOLVE (POINTER) attached to it. This did not seem to cause a problem, I was able to download the GPIO EXAMPLE and enter DEBUG.
So my question and concern is with the WORKSPACES. I also note there is no way to see what WORKSPACE the PROJECTS in currently in while SW4STM32 is open. The SPACE can be changed, but can't be identified through PROPERTIES.
Can anyone speak about this matter with workspaces? The lesson might be; It's probably not good to have two SW4STM32 loaded.