Skip to main content
Visitor II
August 30, 2018
Solved

1M reading range with ST25 - is it possible?

  • August 30, 2018
  • 3 replies
  • 1132 views

Datasheet says these readers support ISO/IEC 15693 standard for vicinity cards. I need a system with high reliability (99%) read for distances up to 1 meter (0.5-0.7 m as the most probable range). Can I use this IC for building such reader alone, or I need additional RF components? What size the antenna should be?

Also, what kind of tags will work best? I can make powered tag as well, but I need min 6 month battery life on something like CR2032.

    This topic has been closed for replies.
    Best answer by Travis Palmer

    Hello,

    Increasing the reading range to 1 meter will likely require to:

    *) adapt the reader antenna size to optimize the power transfer from reader to tag in 1 meter distance

    *) if possible to also adapt the tag antenna size

    *) add an additional amplifier between IC's RFO pins and matching network

    13.56MHz RFID has been developed for proximity operation.

    There are other RFID technologies which are meant to transfer data over larger distances.

    If this would be an option, please have a look at the ST25RU products.

    BR Travis

    3 replies

    ST Employee
    August 31, 2018

    Hello,

    Increasing the reading range to 1 meter will likely require to:

    *) adapt the reader antenna size to optimize the power transfer from reader to tag in 1 meter distance

    *) if possible to also adapt the tag antenna size

    *) add an additional amplifier between IC's RFO pins and matching network

    13.56MHz RFID has been developed for proximity operation.

    There are other RFID technologies which are meant to transfer data over larger distances.

    If this would be an option, please have a look at the ST25RU products.

    BR Travis

    AErofAuthor
    Visitor II
    August 31, 2018

    Thank you. Does ST have reference designs or evaluation kits for such use cases?

    ST Employee
    September 10, 2018

    Hi,

    There are no reference designs or eval kits for ST25R products with more than 1.4W ouput power available.

    BR Travis