About 2.2.4 in datasheet of ST25R3916
Dear Sir,
When I read 2.2.4 in the datasheet, there is a Note as
Using hardware based wake-up in combination with the automatic antenna tuning feature is
not recommended. Contact your nearest ST office for further support.
Could you tell me where I can find more information about the reason?
What kind of wake-up is referred to in this note? is it the low power card detection
mentioned in capacitive sensor (4.2.4)? or Wake-up mode in 4.2.5?
Are the above functions unavailable, if automatic antenna tuning is used?
best regards
Dai