Skip to main content
Visitor II
June 30, 2021
Solved

About the value of MB_MODE of ST25DV64K at power-on

  • June 30, 2021
  • 2 replies
  • 1239 views

Hello all

I use ST25DV64K.

I am always set the MB_MODE of ST25DV64K to 1 after power-on

After setting the value to 1, a verify check is performed to confirm that the value is set to 1.

And the result MB_MODE is 1.

When the power is turned on again after the above operation, MB_MODE is always set to 0.

Since MB_MODE is the "System configuration area", I thought MB_MODE is 1, but MB_MODE is 0.

Is this the correct behavior of the ST25DV?

Also, is there an explanation of this behavior in the datasheet (st25dv64.pdf)?

BR

Morooka

    This topic has been closed for replies.
    Best answer by JL. Lebon

    Hello Morooka,

    The MB_CTRL_Dyn register is a volatile regsiter, and will always be set to 0 at boot time.

    The MB_MODE is a static configuration register that is non-volatile, and value is kept upon reboot.

    Now, the MB_MODE is not linked to the value of MB_EN bit in MB_CTRL_Dyn register.

    Here is how it works:

    If MB_MODE=0, it is forbidden to write in MB_CTRL_Dyn register.

    If MB_MODE=1, it is allowed to write in MB_CTRL_Dyn register.

    MB_CTRL_Dyn is used to enable the mailbox (so called Fast Transfer Mode), on demand during a session, by writing the MB_EN bit to 1.

    By default, the device always boots with mailbox disabled, meaning MB_EN=0 in MB_CTRL_Dyn register.

    So, if you want to use the mailbox after boot, you have to explicitly write MB_EN=1 in MB_CTRL_Dyn.

    Hope this is more clear now.

    Best regards.

    2 replies

    MMoro.4Author
    Visitor II
    July 5, 2021

    I'm sorry.

    The register is not MB_MODE, but MB_EN(bit0) of MB_CTRL_Dyn register.

    So, will the MB_EN bit of the MB_CTRL_Dyn register be set to "0" when the power is turned on?

    Even if the MB_MODE register is '1', will the MB_EN bit in the MB_CTRL_Dyn register remain '0'?

    BR

    Morooka​

    JL. LebonAnswer
    ST Employee
    July 8, 2021

    Hello Morooka,

    The MB_CTRL_Dyn register is a volatile regsiter, and will always be set to 0 at boot time.

    The MB_MODE is a static configuration register that is non-volatile, and value is kept upon reboot.

    Now, the MB_MODE is not linked to the value of MB_EN bit in MB_CTRL_Dyn register.

    Here is how it works:

    If MB_MODE=0, it is forbidden to write in MB_CTRL_Dyn register.

    If MB_MODE=1, it is allowed to write in MB_CTRL_Dyn register.

    MB_CTRL_Dyn is used to enable the mailbox (so called Fast Transfer Mode), on demand during a session, by writing the MB_EN bit to 1.

    By default, the device always boots with mailbox disabled, meaning MB_EN=0 in MB_CTRL_Dyn register.

    So, if you want to use the mailbox after boot, you have to explicitly write MB_EN=1 in MB_CTRL_Dyn.

    Hope this is more clear now.

    Best regards.

    MMoro.4Author
    Visitor II
    July 9, 2021

    Hello JL.Lebon,

    Thank you for your reply.

    I understand about MB_MODE and MB_CTRL_Dyn register.

    Thank you!!

    Morooka