Hello,
Yes, the Icc1 is the current measured on VCC pin, so it is for the whole circuit.
Power consumption down to 1uA can be done by setting the LPD pin to high level.
Please be aware that the LPD pin is available only on the 12-pin package of the ST25DV04K.
About your measurement:
As described in the datasheet, there is different packages available for the ST25DV04K. Some packages have 8-pins, others have 12-pins. As shown in the datasheet, only the 12-pins version have the LPD pin that allows to enter in low power mode.
If you have a ST25DV-Discovery kit for the ST25DV04K, then you have the SO8 package (8-pin package). In this case you don't have the LPD pin, and you can't activate the low power mode.
If you plan to use the ST25DVxxK version, you need to get the 12-pin package. This is available with the X-NUCLEO-NFC04A1 development board (https://www.st.com/en/ecosystems/x-nucleo-nfc04a1.html).
Or you can order the ST25DV64KC-Discovery kit for the ST25DV64KC (newer version of the ST25DVxxK) , which is delivered in the 12-pin DFN12 package and then you can use this one to test the 1uA Low power mode.
If you need to design a low power application with the ST25DV, there is this application note that can help you optimize the power consumption: https://www.st.com/resource/en/application_note/an5733-using-st25dvi2c-series-for-ultralow-power-applications-stmicroelectronics.pdf
Best regards.