(AN5592, ST25R) Differential Antenna with cable
Hello ST Community,
I’m working with the ST25R3911B on a NUCLEO‑NFC08A board and would like to drive a custom differential antenna via two separate coaxial cables. Here is what I’ve done so far and the questions I have:
I disconnected the onboard PCB antenna/cable and wired two 40 cm jumpers to the PCB antenna pads. (X-NUCLEO-NFC08A board)
I was able to run the reader in differential mode, but significant decrease in Rx power due to impedance mismatch caused by wires.
My goal is to design a custom differential PCB antenna and connect it to the ST25R3911B board using coaxial cables, use differential mode to maximize the delivered RF power.
1) Dual‑Coax Differential Connection
I am considering fitting an SMA connector on each of the chip’s RF Output 1 and RF Output 2 pins and likewise two SMAs on my differential antenna. I would then use two 50 Ω coaxial cables to link them.
The AN5592 datasheet only shows a single‑ended coax example.
Is it acceptable to run the ST25R3911B in true differential mode using two separate 50 Ω coax cables and SMA connectors? Any tips or concerns?
2) Alternative: Matching Tool & Non‑Coax Wiring
If the above approach is not recommended, I plan to:
Use ST’s Antenna Matching Tool to design a matching network.
Wire my antenna to the board with simple wire (not coax) and measure the antenna + wire characteristics with a VNA.
Apply the matching network based on those measurements.
Does this workflow make sense?
Thank you for any guidance or suggestions you can provide!