Antenna design, dual tag
Hi gent's
sorry: my first post here, hope everything goes well.
I would like to redesign an antenna for an 95HF, today for test, we use a Nucleo board and it's working pretty well; but I think we can do better.
We need to read 2 tags: one on the Wafer Pod case; one inside the case, on the cassette.
distances are in the range of 10cm but unfortunatelly tag inside Pod is prety at 90°.
I read carefully AN3394 and think I basicaly understood what I should do to adapt impedances;
but now I have to design my antenna according also to the space I have in front...
I saw ther is a 'simplified software tool' (antenne.exe) but I was not able to find it for download.
Any comment, help is welcomme.
Thanks and regards
JMI