Antenna Matching Tool not giving accurate values?
I am new to antenna matching so I decided to use the ST25R Antenna Matching tool V3.1. It seems simple enough, and gave me this output after adding in my antenna parameters (taken right from the datasheet):
However when I simulate this circuit in Qucs, the outputs don't seem like the parameters calculated actually matched the antenna:
I was under the impression that the circuit should be matched in a way so that the target frequency is in a valley of the S11 plot and a peak of the S21 plot. If that's true, is there a parameter or value I'm not setting correctly or do I just need to do the rest by hand?