Can ST Reader read when UHF Antenna and UHF Tag between Woods?
Hello,
I am working with ST25RU3993 Reader and kit's Antenna.
Initially, the Reader was able to detect different Tags using different Antennas. Then, by placing the antenna below a wood surface and tags above the wood surface, the ST UHF Reader was not able to detect any Tags. Later, even at normal conditions (without wood and placing all in a plain surface without any interruption) the Reader did not read any Tags, which worked fine before the above told setup made. I feel the Reader is damaged but not Antenna or Tag. Even after updating ST Reader with new ST Firmware Version 2 and ST GUI Version 2, the Reader did not read any Tags. Byconnecting ST Reader with ST GUI, the LEDs (MCU OK, PLL OK, OSC OK, D16/17, EXT_PA, Tuning, Tuned, RF ON) Turns ON but there is NO TAG RESPONSE. Booting or Reseting or Antenna Tuning neither did not work.
I would like to know where the problem is. Is it with ST Reader, which can not read between Woods?
Kindly help with the same.
Thanks.