Can't Detect IRQ Pin Goin' High Level - ST25RU3993
Hi,
Just started to test a prototype based in the old FENTO Reader Hardware using the AS3993, now AKA ST25RU3993.
I am able to read/write registers using the SPI pins, but I cannot generate an interruption.
I have been trying to execute the interruption using two methods. First Method:
1 -Write 0x20 to Register 0x35 (Enable FIFO Interrupt)
2 - Write 0x03 to Register 0x3D (Set 48 Bytes for Transmission)
3 - Send the Comand 0x90 (Transmission with CRC)
4 - Write 4 bytes to address 0x3F, 6 times (Supplying less bytes to generate an interrupt)
Pin IRQ stays LOW.
Second one:
1 -Write 0x00 to Register 0x35 (Disable All Interrupts in this Register)
2 - Write 0x40 to Register 0x36 (Enable End of Comand Interruption)
3 - Send the Comand 0x87 (Start AD Conversion)
Pin IRQ stays LOW.
This tests are the same ones used by ST and AMS in their sample codes.
I am sure the MCU pin is working correctly and detecting the rising edge in the correct pin. Tested. I am also sure that the IRQ pin is conected to the correct pin in the MCU.
Has anyone some insights of what could be a possible cause for this problem?