Can you suggest an app or method that I can simulate the nfc antenna and see if it works?

I design NFC antenna using ST25TN01K(50pF) chip .This is my first time in RF design. I calculated data with edesignsuit that I shared first photo. Firstly I wonder is my design okay and proper? My design must be small and antenna coil inductance 2.58uH(2nd photo). Both ends of the antenna go directly into the chip.
Apart from these, is there anything else I should pay attention to or add?
Can you suggest an app or method where I can simulate the nfc antenna and see if it works?