cannot detect any tag on ST25R3916
Hi,
I have made a custom design for reading/writing NTAG213 tags based on the X-NUCLEO-NFC06A1 board. I have adapted the firmware that works on this demo board (along with all the drivers related to the ST25R3916 and RFAL) into a STM32G030K8T6 microcontroller.
I have neither capacitive sensing nor AAT implemented in Hardware and I have also disabled these mechanisms in the Firmware according to this post.
The antenna design is very similar to the ST25R3916 Discovery Board (2 turns, 65mm x 85 mm). For the the antenna analysis I have measured its real parameters following the indications of the AN5276 Application Note:
This is LANT = 1.03 uH RSDC = 440m Ohms fres = 60.19 MHz Rp @ fres = 7.29 Kohms
Buy using the ST25R Antenna Matching Tool I get the following values for the custom board:
On the Firmware side the Initialization is successful (ERR_NONE)... but does not detect any tag during execution of the detection cycle routines.
I have checked the presence of any signal near the antenna by means of a small loop made with the oscilloscope probe. I see that the antenna is actually emitting at 13.56MHz every second.
Everything seems to be correct but why can't I detect any tag?
gaston