Skip to main content
Explorer
March 15, 2023
Solved

code to read and write NDEF on X-NUCLEO-NFC07A1

  • March 15, 2023
  • 2 replies
  • 1240 views

Can the following code be used to enable the phone to read and write NDEF messages?

I use X-NUCLEO-NFC07A1 and NUCLEO-L476RG

/* USER CODE BEGIN Header */
 
/**
 
 ******************************************************************************
 
 * @file : main.c
 
 * @brief : Main program body
 
 ******************************************************************************
 
 * @attention
 
 *
 
 * Copyright (c) 2021 STMicroelectronics.
 
 * All rights reserved.
 
 *
 
 * This software is licensed under terms that can be found in the LICENSE file
 
 * in the root directory of this software component.
 
 * If no LICENSE file comes with this software, it is provided AS-IS.
 
 *
 
 ******************************************************************************
 
 */
 
/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
 
#include "main.h"
 
#include "app_nfc7.h"
 
#include "lib_NDEF.h"
 
/* Private includes ----------------------------------------------------------*/
 
/* USER CODE BEGIN Includes */
 
 
 
 
 
 
 
/* USER CODE END Includes */
 
 
 
/* Private typedef -----------------------------------------------------------*/
 
/* USER CODE BEGIN PTD */
 
 
 
/* USER CODE END PTD */
 
 
 
/* Private define ------------------------------------------------------------*/
 
/* USER CODE BEGIN PD */
 
/* USER CODE END PD */
 
 
 
/* Private macro -------------------------------------------------------------*/
 
/* USER CODE BEGIN PM */
 
 
 
/* USER CODE END PM */
 
 
 
/* Private variables ---------------------------------------------------------*/
 
 
 
/* USER CODE BEGIN PV */
 
 
 
/* USER CODE END PV */
 
 
 
/* Private function prototypes -----------------------------------------------*/
 
void SystemClock_Config(void);
 
static void MX_GPIO_Init(void);
 
/* USER CODE BEGIN PFP */
 
 
 
/* USER CODE END PFP */
 
 
 
/* Private user code ---------------------------------------------------------*/
 
/* USER CODE BEGIN 0 */
 
 
 
/* USER CODE END 0 */
 
 
 
/**
 
 * @brief The application entry point.
 
 * @retval int
 
 */
 
int main(void)
 
{
 
 /* USER CODE BEGIN 1 */
 
 uint8_t data[] = "Hello, world!";
 
 // 创建NDEF消�?�
 
 NDEF_WriteNDEF(strlen((char *)data), data);
 
 //读�?�NDEF消�?�
 
 NDEF_ReadNDEF(data);
 
 
 
 /* USER CODE END 1 */
 
 
 
 /* MCU Configuration--------------------------------------------------------*/
 
 
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 
 HAL_Init();
 
 
 
 /* USER CODE BEGIN Init */
 
 
 
 /* USER CODE END Init */
 
 
 
 /* Configure the system clock */
 
 SystemClock_Config();
 
 
 
 /* USER CODE BEGIN SysInit */
 
 
 
 /* USER CODE END SysInit */
 
 
 
 /* Initialize all configured peripherals */
 
 MX_GPIO_Init();
 
 MX_NFC7_Init();
 
 /* USER CODE BEGIN 2 */
 
 
 
 /* USER CODE END 2 */
 
 
 
 /* Infinite loop */
 
 /* USER CODE BEGIN WHILE */
 
 while (1)
 
 {
 
 
 
 /* USER CODE END WHILE */
 
 
 
 MX_NFC7_Process();
 
 /* USER CODE BEGIN 3 */
 
 }
 
 /* USER CODE END 3 */
 
}
 
 
 
 
 
/**
 
 * @brief System Clock Configuration
 
 * @retval None
 
 */
 
void SystemClock_Config(void)
 
{
 
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 
 
 /** Configure the main internal regulator output voltage
 
 */
 
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 
 {
 
 Error_Handler();
 
 }
 
 /** Initializes the RCC Oscillators according to the specified parameters
 
 * in the RCC_OscInitTypeDef structure.
 
 */
 
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 
 RCC_OscInitStruct.PLL.PLLM = 1;
 
 RCC_OscInitStruct.PLL.PLLN = 10;
 
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 
 {
 
 Error_Handler();
 
 }
 
 /** Initializes the CPU, AHB and APB buses clocks
 
 */
 
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 
 {
 
 Error_Handler();
 
 }
 
}
 
 
 
/**
 
 * @brief GPIO Initialization Function
 
 * @param None
 
 * @retval None
 
 */
 
static void MX_GPIO_Init(void)
 
{
 
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 
 
 /* GPIO Ports Clock Enable */
 
 __HAL_RCC_GPIOC_CLK_ENABLE();
 
 __HAL_RCC_GPIOH_CLK_ENABLE();
 
 __HAL_RCC_GPIOA_CLK_ENABLE();
 
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 
 
 /*Configure GPIO pin Output Level */
 
 HAL_GPIO_WritePin(GPIOA, LD2_Pin|GPIO_PIN_10, GPIO_PIN_RESET);
 
 
 
 /*Configure GPIO pin Output Level */
 
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4|GPIO_PIN_5, GPIO_PIN_RESET);
 
 
 
 /*Configure GPIO pin : B1_Pin */
 
 GPIO_InitStruct.Pin = B1_Pin;
 
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
 
 
 
 /*Configure GPIO pins : USART_TX_Pin USART_RX_Pin */
 
 GPIO_InitStruct.Pin = USART_TX_Pin|USART_RX_Pin;
 
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 
 GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
 
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 
 
 /*Configure GPIO pins : LD2_Pin PA10 */
 
 GPIO_InitStruct.Pin = LD2_Pin|GPIO_PIN_10;
 
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 
 
 /*Configure GPIO pin : PA6 */
 
 GPIO_InitStruct.Pin = GPIO_PIN_6;
 
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 
 
 /*Configure GPIO pins : PB4 PB5 */
 
 GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;
 
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
 
 
 /* EXTI interrupt init*/
 
 HAL_NVIC_SetPriority(EXTI9_5_IRQn, 0, 0);
 
 HAL_NVIC_EnableIRQ(EXTI9_5_IRQn);
 
 
 
}
 
 
 
/* USER CODE BEGIN 4 */
 
 
 
/* USER CODE END 4 */
 
 
 
/**
 
 * @brief This function is executed in case of error occurrence.
 
 * @retval None
 
 */
 
void Error_Handler(void)
 
{
 
 /* USER CODE BEGIN Error_Handler_Debug */
 
 /* User can add his own implementation to report the HAL error return state */
 
 __disable_irq();
 
 while (1)
 
 {
 
 }
 
 /* USER CODE END Error_Handler_Debug */
 
}
 
 
 
#ifdef USE_FULL_ASSERT
 
/**
 
 * @brief Reports the name of the source file and the source line number
 
 * where the assert_param error has occurred.
 
 * @param file: pointer to the source file name
 
 * @param line: assert_param error line source number
 
 * @retval None
 
 */
 
void assert_failed(uint8_t *file, uint32_t line)
 
{
 
 /* USER CODE BEGIN 6 */
 
 /* User can add his own implementation to report the file name and line number,
 
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 
 /* USER CODE END 6 */
 
}
 
#endif /* USE_FULL_ASSERT */

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi,

    calling NDEF_WriteNDEF or NDEF_ReadNDEF before the various initialization cannot work.

    I would suggest to have a look to MX_NFC7_Init and to customize it to fit with your needs.

    Rgds

    BT

    2 replies

    Technical Moderator
    March 21, 2023

    Hi,

    calling NDEF_WriteNDEF or NDEF_ReadNDEF before the various initialization cannot work.

    I would suggest to have a look to MX_NFC7_Init and to customize it to fit with your needs.

    Rgds

    BT

    SchuylerAuthor
    Explorer
    March 22, 2023

    Hi,

    I know what you mean and I've been to see it. If I insert NDEF_WriteNDEFand NDEF_ReadNDEF after MX_NFC7_Init such as between/* USER CODE BEGIN 2 */ and /* USER CODE END 2 */, Can I enable the phone to read and write NDEF messages?