Continues data Transmission with i²c
Is it possible to transfer large data files, meaning bigger than the internal memory of the tag?
The intended purpose is to have a stm32 connected to an i²c dynamic tag and be able to write large files, like a new firmware, to the stm32 MCU. The problem is, that I couldn't find documentation if it is possible to simultaneously read the data via i²c which is currently written to the tag via NFC. If not possible in a continues stream, reading in chunks would be a viable alternative. As long as it is possible to do in one NFC "Session". That would allow a 0 port device that can be sealed towards the environment.