CR95HF and DESFire
Posted on April 21, 2014 at 05:45
Hi Everyone,
I'm using the CR95HF to access the DESFire card. Everything was going fine up to RATS and PPS.
However when I tried to send the GetVersion Desfire command (0x60) using the Half-duplex block transmission protocol with PCB, CID, INF... as below:
0x04, 0x04, 0x0A, 0x00, 0x60, 0x28
header, len, PCB, CID, INF, control byte
I only received 0x87 0x00. The same happened with Authenticate (0x0A 0x00) command. So I think I it must be something wrong with the EDC (CRC) code.
Could anybody shed some light on this?
--------------------------------------------------
Edited: According to the datasheet, the CR95HF only supports 14443-3 not 14443-4, is that correct?
#desfire #cr95hf