CR95HF Data Rate, Subcarrier and 10%/100% Modulation Parameters
I've been using the M24LR-Discovery kit to evaluate the read range to our 15693 tags. My measurements are in the 2.6 inch to 3.5 inch range, depending on how I set the Data Rate and subcarrier settings. The best range is achieved with 'LOW' date rate, and no subcarrier. The 10%/100% modulation setting has no effect on range as far as I see.
Are there reasons to NOT use LOW date rate and NO subcarrier for our reader?
How should I determine to use 10% or 100% modulation?
Thanks!