CR95HF file NDEF not found
Dear Sir/Madame,
I am using X-NUCLEO-NFC03A1 connected to our MCU (NXP Kinetis). The communication protocol used is SPI and it works well (sends and receives echo). Therefore, we would like to read a text on the smartphone in "NDEF tag emulator" mode, but in the reponses indicate that the NDEF file is not found.
Our goal is to deesign an access control with an NFC reader that is accesser with a smartphone application.
The commands used are extracted using the datasheet, page 78-81, D.1.5 Forum Tag Type 4A, and it works well until the commands after "Select Application" because it responds 0x6A 0x82 (file or application not found). The Select application responds 0x90 0x00 0xF1 0x00, but if I change the command to >>> CR95HFDLL_SENDRECV, 02 00 A4040007D276000085010100 28, it responds 0xF2 (I understand that the timeW is exceeded and I put the maximum value 0x60).
Could you please help us to solve this situation?
Thanks you and Best regards,
José Manuel.-