CR95HF Linux kernel driver
Hi,
I am working on linux kernel v4.19 to bring up the cr95hf via SPI, there is a existing driver called st95hf, I enabled it, and it can be probed. can get ECHO back.
when I used nfc neard to test the driver, it always gives errors like below:
[ 501.027260] spi_geni 988000.spi: Zero length transfer
[ 501.027307] st95hf spi1.0: SPI transfer failed: -22
[ 501.027393] spi_master spi1: failed to transfer one message from queue
[ 501.027436] st95hf spi1.0: spi_recv_resp, data read error = -22
[ 501.027471] st95hf spi1.0: spi error from st95hf_spi_recv_response(), err = 0xffffffea
[ 501.027506] nfc nfc0: protocol sel send field off, err = 0xffffffea
[ 501.036499] digital: digital_in_configure_hw: in_configure_hw failed: -22
[ 501.037971] spi_geni 988000.spi: Zero length transfer
[ 501.038042] st95hf spi1.0: SPI transfer failed: -22
[ 501.038181] spi_master spi1: failed to transfer one message from queue
[ 501.038246] st95hf spi1.0: spi_recv_resp, data read error = -22
[ 501.038298] st95hf spi1.0: spi error from st95hf_spi_recv_response(), err = 0xffffffea
[ 501.038351] nfc nfc0: protocol sel send field off, err = 0xffffffea
[ 501.048640] digital: digital_in_configure_hw: in_configure_hw failed: -22
[ 501.050030] spi_geni 988000.spi: Zero length transfer
[ 501.050090] st95hf spi1.0: SPI transfer failed: -22
I would like to know is there any verified cr95hf driver for linux kernel?