Skip to main content
Visitor II
November 17, 2020
Solved

Decoupling capacitors for ST25R3911B

  • November 17, 2020
  • 2 replies
  • 1038 views

Hi.

The datasheet of ST25R3911B shows recommended values of capacitors of 1uF (for AGD/VSS) and 2.2uF for others (VSPx-VSNx) plus a 10nF capacitor very close to the pins, according to the the picture:

0693W000005BfuvQAC.pngI just wanted to know if I should use these exact values, or if I can start my custom board project using 4.7uF/0402 for all these 1uF and 2.2uF capacitors. We already have the 4.7uF/0402 in stock. Just wanted to know if I can use them instead of 1uF/2.2uF values recommended on the datasheet. And also if I can use 4.7uF+10nF on VDD pin

    This topic has been closed for replies.
    Best answer by Travis Palmer

    Hello JPehl,

    The values from the datasheet above are those which we used for our reliability testing of the IC. Only if these values are used, the values in chapter 3 "Electrical characteristics" of the datasheet are guaranteed by ST. AGD for example is the Analog Reference. It is being driven or powered-down during operation and low power mode. Using different capacitor values could cause different rise times and therefore malfunctions.

    BR Travis.

    2 replies

    ST Employee
    December 1, 2020

    Hello JPehl,

    The values from the datasheet above are those which we used for our reliability testing of the IC. Only if these values are used, the values in chapter 3 "Electrical characteristics" of the datasheet are guaranteed by ST. AGD for example is the Analog Reference. It is being driven or powered-down during operation and low power mode. Using different capacitor values could cause different rise times and therefore malfunctions.

    BR Travis.

    JPehl.1Author
    Visitor II
    December 1, 2020

    Hi Travis.

    Ok, I will use recommended values only.

    But on VDD pin, whats the best combination?

    • 100nF + 2.2uF ?
    • 100nF + 1uF ?

    Regards,

    Jeferson.

    ST Employee
    December 4, 2020

    Hi Jeferson,

    on VDD i would also stick to 10nF + 2.2uF. You can also check the schematics of our demo kits. They should have the same decoupling components as mentioned in the datasheet.

    br Travis

    JPehl.1Author
    Visitor II
    December 4, 2020

    About the "bulk" capacitor for VDD, there is no indication on the datasheet. The development board uses 1uF, but you recommended 2.2uF, and I would stick to 2.2uF also. So I will use 100nF + 2.2uF.

    Thanks and regards,

    Jeferson