Decrease the time to write/read a block fro a NFC Tag
Hello,
I'm using the X-Nucleo-NFC08A1 with the X_Cube NFC 6 and a NFC(V - ISO15693) Tag. I want to decrease the time for reading and writing. I also want do decrease the time for detecting a Tag. Are their any parameters to change or is the speed highly dependent on the Tag.
I already lwered the discParam.totalDuration to 10ms and turned off all functions that work with a different type of Tag.
Time to read a single Block: 11.38 ms
Time to write a single Block: 15.65 ms
Thank you for helping
Rgds