Design & Match a Wire-Wound Antenna (Air Coil) for ST25TV02KC with ST25R3916B ?
Hi everyone,
I'm currently working on an NFC reader design using the ST25R3916B in single-ended configuration to read and write ST25TV02KC tags (ISO15693, NFC-V).
Instead of a PCB antenna, I'm using a round, wire-wound air coil antenna and now need to properly design the antenna and match it to the reader IC.
My questions are:
How do I correctly design a wire-wound (air coil) antenna for 13.56 MHz in this setup? Should the antenna's resonance frequency be at ~13,56MHz or including the antenna network circuit (--> f_0 of antenna >13.56MHz)?
Which parameters (e.g. inductance, Q, ...) are most important to measure or calculate for use in the ST matching tools?
The STM32 NFC Inductance Tool seems to be designed for PCB trace antennas – can it be used for air coils as well, or should I rely on external tools? The resonance frequency of the antenna must be ~13.56MHz?
How do I calculate or match the antenna network correctly for single-ended use with the ST25R3916B, once I have the coil parameters? Resonance frequency including antenna must be ~13,56MHz? Or must the antenna have by itself a resonance frequency of ~13.56MHz?
Any help or clarification on how to approach this would be greatly appreciated – especially from those who have worked with non-PCB antennas in combination with ST's design tools.
Thanks in advance!
Best regards