Designing ST25DV64K antenna
Hi,
We want to design an antenna for the ST25DV64K NFC chip. According to the characteristics that the chip has, it needs an antenna with an inductance of 4,83 uH. Our question is if we can design an antenna with higher inductance and add a series capacitor to the chip to compensate. For example: if we create a 12.69 uH antenna, the capacitance of the chip should be 10.85 pF (ST25DV64K chip internal capacitance is 28,5 pF). Can we add a 17.52 pF series capacitor to the chip to achieve the desired capacitance? Or is it only possible to add capacitors in parallel? Thank you for the help.
Best regards,
IF