Skip to main content
Graduate
August 27, 2025
Solved

Determining output power from the ST25R3916

  • August 27, 2025
  • 2 replies
  • 289 views

Is there a way to find the RF output power using the ST25R3916 without measuring it externally? I don't need an exact value. 

The product selector says the nominal output power is 1600 mW. However, at a max of 3 Vpp and 150 mA input current (measured via power profiler), that's 450 mW not including losses. I know that the output power can be adjusted via the d_res register, which I do, but that's only to aim for the target amplitude. Is there something else I can look at here?

    This topic has been closed for replies.
    Best answer by Ulysses HERNIOSUS

    Hi,

    output power needs to be measured externally.

    BR, Ulysses

    2 replies

    Technical Moderator
    August 28, 2025

    Hi,

    output power needs to be measured externally.

    BR, Ulysses

    LltWcAuthor
    Graduate
    August 28, 2025

    Got it, thanks