Posted on March 06, 2018 at 13:14Hi Joseph,
The ST25R3911B has some features build in to overcome environmental changes in wake-up mode.
Automatic Averaging for example can be used to filter slow changing effects like temperature change or changing humidity. Only 'fast' changes like detuning by a tag or phone will be recognized.
The delta-window is another setting that changes the sensitivity of the wake-up feature. It allows to set a range around the reference value, where no interrupt is triggered.
An interrupt can also be triggered by another device which operates at the same frequency range. A BLE or WIFI device is too different in terms of frequency to generate an amplitude change on the IC's input pins. A phone which also sends out actively an HF field @ 13.56MHz will interfere with the inductive wake-up pulse and therefore also trigger an interrupt when being active in closer proximity.
BR Travis