Skip to main content
Visitor II
May 29, 2023
Solved

Editing ST25R3911B DISCO in STM32CubeIDE

  • May 29, 2023
  • 7 replies
  • 2479 views

Editing ST25R3911B DISCO in STM32CubeIDE did not generate an error, but it cannot be read. How can ST25R3911B edit NFC in STM32Cube?

    This topic has been closed for replies.
    Best answer by Brian TIDAL

    Hi:

    The X-NUCLEO-NFC05A1 is an NFC card reader expansion board based on the ST25R3911B.

    See X-NUCLEO-NFC05A1, UM2252, X-CUBE-NFC5 and UM2253

    Rgds

    BT

    7 replies

    Technical Moderator
    May 29, 2023

    Hi

    STSW-ST25R002 Firmware for ST25R3911B-DISCO kit (Source) is provided with a Keil µVision project file. The support of STM32Cube is not provided.

    If you are looking for a development board with FW package available for STM32Cube, I would rather recommand to use the X-NUCLEO-NFC05A1 board and the X-CUBE-NFC5 FW package.

    Rgds

    BT

    Gfang.2Author
    Visitor II
    May 29, 2023

    Can the X-NUCLEO-NFC05A1 board serve as a reader for reading data?

    Technical Moderator
    May 29, 2023

    Hi:

    The X-NUCLEO-NFC05A1 is an NFC card reader expansion board based on the ST25R3911B.

    See X-NUCLEO-NFC05A1, UM2252, X-CUBE-NFC5 and UM2253

    Rgds

    BT

    Gfang.2Author
    Visitor II
    June 6, 2023

    I am currently using X-NUCLEO-NFC05A1. Can I use X-CUBE-NFC7 to configure ST25?

    Technical Moderator
    June 6, 2023

    Hi,

    the FW package for the X-NUCLEO-NFC05A1 is X-CUBE-NFC5 not X-CUBE-NFC7.

    Rgds

    BT

    Gfang.2Author
    Visitor II
    June 7, 2023

    Can STM32Cube add X-CUBE-NFC5? If possible, how can I add X-CUBE-NFC5?