Errors while compiling the FW STSW-ST25R011 of the “ST25R3916 Discovery Kit ?.
Dear STCommunity members,
I’d like to test the MB1414 (ST25R3916_Discovery_DB) using the I2C interface. So, besides changing the Hardware of the MB1414 (by changing J200, J201, J202, J203, J204 and J205) I also need to update the Firmware of the MB1396 (ST25_Discovery_Mboard) to implement this interface.
For a couple of days, I’ve been trying to compile the FW STSW-ST25R011 provided for the “ST25R3916 Discovery Kit�?, but unfortunately, without success. Probably I am committing a silly mistake since I am not really familiar with this environment.
I am using the Atolic TrueStudio V9.3 to compile it, but after using the Import Wizard to import the “Existing Projects into Workspace�? and “Build Project�? I am getting the following error/warnings (see details attached: “Build_Log_fatal_error.txt�?):
fatal error: stm32l4xx_hal.h: No such file or directory – despite the fact that its include folder is correctly added in the “include directories�? (see details attached: “Screenshot Path and Symbols .png�?).
Obs.: I also tried to compile it using the STM32Cube IDE V1.10 without success.
1- Could you please help me to compile this FW?
2- Could you please tell me which parameter in the FW should I change in order to set the I2C communication in place of the SPI?
Many thanks.