FIELD RISING and FIELD FALLING Interrupt flags are set simultaneously irrespective of direction of movement of reader with respect to st25dv tag
Hello,
I am working on project where I need to check if field is falling or rising. I have enabled the filed change interrupt in GPO, which works fine to generate the GPO interrupt. Unfortunately both the interrupt flags for field change interrupt i.e. field falling and field rising interrupt flags are set irrespective of whether reader is moved towards the tag or away from the tag.
Is this the general case that both the flags are set on field change interrupt?
If not then is there any setting which can be used to control the flag being set?
Any help would be much appreciated!