Getting lots of ST25RU3993_ERR_PREAMBLE and ST25RU3993_ERR_RXCOUNT errors during round
Hello,
I´m testing the ST25RU3993 Eval Board with it´s firmware and I receive lots of ST25RU3993_ERR_PREAMBLE and ST25RU3993_ERR_RXCOUNT errors during inventory round.
My setup contains 72 Tags, all visible for the antenna. (another Reader detects about 70 per Round) If I set a non adaptive Q to 1024 slots I thougt to get about 952 empty slots, maybe some collisions and something about 72 Tags. But instead I find something between 10-62 Tags, something about 450 Empty Slots and 500 Collisions, caused by the two errors I said above. (more by preamble, less by rxcount and a few caused by others (the else in your commented debug print in gen2.c gen2SearchForTags())
I already checked the RXWAITTIME register (0x08) and the RXNORESPONSE Register (0x07), they are on default value.
A problem resulting of that errors is the adaptive Q. Because of the ST25RU3993_ERR_PREAMBLE errors the q increases a lot during round, but it should decrease because of the Empty slots...
Can you tell me what can be my problem?
Thank you very much,
Julien