Skip to main content
Explorer
July 25, 2019
Solved

Hello! I'm using the Workbench Systems on a Mac. I downloaded FP-SNS-SMARTAG1, imported a project for SMARTAG1 to Workbench, but I do not have the Build button active

  • July 25, 2019
  • 1 reply
  • 846 views

0690X000009Z5cMQAS.png

    This topic has been closed for replies.
    Best answer by Salvatore Curti

    Hi,

    I verified that the project with the latest version of the SW4STM32 for MAC is ok (the build button is active and the project build without errors).

    One note:

    • the project for SW4STM32 there is for only nucleo project.
    • binary generated by SW4STM32 for STEVAL-SMARTAG1 is more than the flash dimension, so due to flash size constraints the SW4STM32 project is removed for STEVAL-SMARTAG1
      • the build button for STEVAL-SMARTAG1 is not active because the project there is not in the package.

    It is a known issue, as you can read in the release note:

    ISSUE

    • Due to flash size constraints on STEVAL-SMARTAG1:
      • UART is not available
      • Binary generated by System Workbench for STM32 is not available (the IDE project is removed)
      • Debug mode is not available.

    Regards,

    Salvatore Curti.

    1 reply

    ST Employee
    September 2, 2019

    Hi,

    I verified that the project with the latest version of the SW4STM32 for MAC is ok (the build button is active and the project build without errors).

    One note:

    • the project for SW4STM32 there is for only nucleo project.
    • binary generated by SW4STM32 for STEVAL-SMARTAG1 is more than the flash dimension, so due to flash size constraints the SW4STM32 project is removed for STEVAL-SMARTAG1
      • the build button for STEVAL-SMARTAG1 is not active because the project there is not in the package.

    It is a known issue, as you can read in the release note:

    ISSUE

    • Due to flash size constraints on STEVAL-SMARTAG1:
      • UART is not available
      • Binary generated by System Workbench for STM32 is not available (the IDE project is removed)
      • Debug mode is not available.

    Regards,

    Salvatore Curti.