How to access ST25DV registers on iOS using React Native if NfcV is not supported?
I am working on a React Native project for an NFC app that needs to run on both iOS and Android. I am using the react-native-nfc-manager library to perform NFC operations. The NFC tag I am using is ST25DV, which supports NDEF and NfcV (ISO15693) technologies.
In my app, I need to perform:
- Writing different types of NDEF messages (URI, AAR, etc.).
- Writing directly to static registers (e.g., RFA1SS, ENDA1, RF_PWD_1, etc.).
For writing to registers, I need to access raw memory blocks, which requires NfcV commands.
According to the react-native-nfc-manager documentation, NfcV is not supported on iOS. That leaves me only with NDEF, as the tag only supports NDEF and NfcV.
My questions:
Is there any way to access or write to those registers on iOS without NfcV?
Is there a workaround to enable or simulate NfcV support on iOS?
Or am I limited to NDEF-only operations on iOS with this tag?
Here’s a snippet from my current code that uses NfcV to write a static register (works on Android) I haven't tested that code on iOS yet (as I haven't setup React Native on mac yet for iOS development)
```
await NfcManager.requestTechnology(NfcTech.NfcV); const tag = await NfcManager.getTag(); const res = awaitr NfcManager.transceive([ 0x02, // Request Flag 0xA1, // Command Code for Write Config Register 0x02, // IC Mfg Code fot ST25DV 0x09, // Pointer Address of ENDA1 register 0x3F, // Value of ENDA1 ]);
```