How to configure ST25R3916 stream mode for custom protocol card emulation
The description of the ST25R3916 states "Special stream and transparent modes of the AFE and framing system can be used to implement other custom protocols in reader or card emulation mode." - this makes it sound like it should be possible to implement custom protocols using the stream mode for card emulation.
Unfortunately looking at the datasheet the mode definition register operating modes table only lists stream mode options when the chip is configured as an initiator, there are no stream modes listed when in passive target mode.
Is there a way to leverage stream mode when in card emulation mode, or is transparent mode the only option here (which would seem odd as other posts on the community from ST made it sound like stream mode is preferred over transparent and that transparent mode really only exits for internal testing)?