Skip to main content
Visitor II
June 30, 2021
Solved

How To kill a TAG ?

  • June 30, 2021
  • 1 reply
  • 1774 views

I try to Kill a TAG, I'm using different configurations but don't obtain a different answer.

I believe if a Kill a Tag, It's not more possible for my reader to identify her, but after I using the kill command my Tags still read by my reader.

I want to understand whats means the parameters RFU and RECOM in the struct of the kill. What the values that parameters expected?

What means the error "ERR_GEN2_REQRN"?

0693W00000BcU7sQAF.png

Best Regards.

    This topic has been closed for replies.
    Best answer by Bart Herse

    Hi GPaiv.1,

    did you assign a kill password before sending the Kill command? The Kill command does not work for a zero password.

    RFU means reserved for future use. The kill command has a 3 bit wide field which is called RFU and these bit shall all be zeros.

    RECOM is a dormant piece of code as in the latest Gen2V2 or ISO 18000-63 standard recommissioning of tags is not supported anymore.

    ERR_GEN2_REQRN defines the return code in case an error happens while sending the ReqRN command.

    Cheers,

    B

    1 reply

    Visitor II
    July 16, 2021

    Hi GPaiv.1,

    did you assign a kill password before sending the Kill command? The Kill command does not work for a zero password.

    RFU means reserved for future use. The kill command has a 3 bit wide field which is called RFU and these bit shall all be zeros.

    RECOM is a dormant piece of code as in the latest Gen2V2 or ISO 18000-63 standard recommissioning of tags is not supported anymore.

    ERR_GEN2_REQRN defines the return code in case an error happens while sending the ReqRN command.

    Cheers,

    B