I2C and GPO pin max input voltage
I am using ST25DV04KC tag and using the V_EH pin to power the VCC of the tag only( It will generate around 3.3V which is enough to power up the tag in I2C mode I believe) . I am looking for guidance on the maximum pullup voltage on the I2C and GPO line from an external rail of around 3.6V, if it is okay? what can be the max voltage on the I2C and GPO pins? is it independent of VCC or dependent on VCC?