Solved
i2c present password command
Posted on July 28, 2016 at 11:38
Hello,
I want to modify sector security status area to lock all sectors against RF access (R/W)To do so, I have to send a I2C present password command and then write the sector security status area.I never set the i2c password, so it should be 0000 0000hBut after presenting this password, I can't modify sector security status area.The sector security status area is still the same (I can read it)Is it possible to have a sample code or/and other documentation than AN3002 Description of the M24LRxx-R....Thank you!