Icc figure for M24SR02-Y
I am experiencing spurious lockups of the I²C interface of an M24SR02-Y (see a separate post). Due to time/development constraints, it may be the easiest to simply cycle power to the device when this problem is detected. The datasheet is, however, not completely clear (to me) on supply current requirements.
Is the Icc in Table72 ("RF supply current) stated as 100mA only present in the AC0-AC1 circuit?
The name "Icc" seems to imply that it is through the Vcc pin of the chip, which would mean that we could not supply the device from a microcontroller I/O pin.
Or is the Vcc supply current only the I²C supply current Icc1 as indicated on Table 76 i.e. max of between 200µA and 250µA? If that is the case, then direct supply from a microcontroller I/O pin would be fine.