identical RFID chip at external interface on ST25RU3993 EVAL board
Hello ST and users
In the ST25RU3993 EVAL boared, the micro controller interacts with the RFID reader chip through SPI interface and control signals ( 93_signals) - altogether six data lines in total. The SPI interface is also shared with a carrier cancellation chip.
We wish to add an identical RFID chip and PCB externally through external interfaces ( SPI and 93_signals) and disable/not use the on-board RFID reader chip. This would perhaps allow us to use the already available firmware/GUI for this development kit and we could reduce efforts in Firmware development.
Is such an approach feasible ? what are the consequence on the micro Controller and its re-programming ? is there an application notes for something similar
Thanks and best