Invalid command code error while performing Write operation from C# based PC software application
Hello,
We currently have a desktop application based on C# for communicating between ST25R3911B-DISCO board and ST25DV dynamic tag. The application itself is similar to ST PC software for ST25R3911B-DISCO board but with limited functionalities as currently we only need Fast Transfer Mode for communication.
My PC software based on C# is able to perform inventory discovery successfully, and is also able to read the data from mailbox (verified by writing data to mailbox using ST software and reading data by using C# software). But issue arrives when i try to perform Mailbox write operation, the error returned is invalid command code for write operation. I looked at the ST25DV datasheet for RF commands and frame formats also the logs of the ST PC software to understand how the write operation data frame is transmiited but that's different from the data frame that's sent from my application. There are files in my project which adds the protocol header to data frame.
So can anyone please help me what could be the issue here. I have added the payload that sent from my application to ST25DV dynamic tag for both read and write operation below:
Here is the frame format that's sent for read operation which is working:
READ:
--------------------
0F-15-00-44-00-10-04-40-DE-00-0C-22-AC-02-81-38-3F-05-00-25-02-E0-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
1st byte is counter
AC - read cmdHere is the frame format that's sent for write operation which is not working and throwing error of invalid cmd:
WRITE :
--------------------
01-18-00-44-00-13-04-40-DE-00-0C-22-AA-02-81-38-3F-05-00-25-02-E0-04-FF-FF-FF-FF-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
1st byte is counter
AA - write cmd
04 - data length
FF-FF-FF-FF - dataNOTES:
In both write and read packets, (4-5)bytes before CMD code is same (i.e "40-DE-00-0C-22") and bytes after CMD code is same (i.e "02-81-38-3F-05-00-25-02-E0")
So can you please let me know what could be the possible reason why i am getting this invalid command error, although my command is right.