Skip to main content
Visitor II
November 3, 2017
Solved

is it possible to connect more than one RFDemo Board and use them asynchronously ?

  • November 3, 2017
  • 1 reply
  • 570 views
Posted on November 03, 2017 at 15:30

Hello, I'm using the RF Transceiver Demonstration Board, I connected it via USB, I successed in writing labview code that  read/write messages via NFC to a device.

My question is: is it possible to connect more than one Demo Board and use them asynchronously ? I need to read/write NFC messages at least to two devices at the same time.

Thank you

Regards.

Massimo Ponte

#m24lr-discovery
    This topic has been closed for replies.
    Best answer by NFC/RFID Customer support
    Posted on December 15, 2017 at 17:02

    Hi Massimo,

    If your question is about CR95HF-DEMO kit (embedded in the M24LR-DISCOVERY kit), it is not possible to use 2 readers via USB ports.

    Best regards

    1 reply

    ST Employee
    December 15, 2017
    Posted on December 15, 2017 at 17:02

    Hi Massimo,

    If your question is about CR95HF-DEMO kit (embedded in the M24LR-DISCOVERY kit), it is not possible to use 2 readers via USB ports.

    Best regards