Is ST25R3911B compatible with AMS AS3955 dynamic tag?
Hello,
I am working on a project based on NFC energy harvesting application. I am using AMS AS3955 dynamic tag which offers this functionality with ST25R3911B as the reader. In the ST25R3911B datasheet, it says that NFC type 4 tags are preferred and nothing is mentioned about other tag types.
Can ST25R3911B work with T2T commands(read/write)? If no then please suggest an alternative.
PS: AS3955 can also work on ISO14443A standard, but its mode must be changed to tunneling.
Thank you in advance!