Skip to main content
Visitor II
November 11, 2019
Solved

Is ST25RU3993 suitable for long distance readings?

  • November 11, 2019
  • 2 replies
  • 908 views

Ps: I saw https://community.st.com/s/question/0D50X0000BWnXe0SQF/st25ru3993-antenna , but it was not enough.

I'm interested in testing the https://www.st.com/en/nfc/st25ru3993.html , but I couldn't find information concerning antenna support. Have anyone used this module to accomplish long distance UHF readings? Can I achieve it with ST25RU3993?

I'm searching for

  • a long distance UHF reader, 2 Km <= kilometres <= 10 Km ;
  • a "not so short" distance UHF reader, 2 m <= meters <= 10 m;

Which antennas have you used? Everything goes well?

Thanks!

    This topic has been closed for replies.
    Best answer by Bart Herse

    ​Hello,

    I am sorry, but for a read range between 2 km and 10 km I would suggest to look into a different kind of technology for sure it should be some kind of active tech.

    ST25RU3993 can well support reader for ranges between 2 and 10 meters.

    Cheers,

    B

    2 replies

    Visitor II
    November 19, 2019

    ​Hello,

    I am sorry, but for a read range between 2 km and 10 km I would suggest to look into a different kind of technology for sure it should be some kind of active tech.

    ST25RU3993 can well support reader for ranges between 2 and 10 meters.

    Cheers,

    B

    jcbrtlAuthor
    Visitor II
    November 19, 2019

    Hello Bart,

    Thank you for the answer.

    As far as I'm concerned, the module doesn't come with an antenna,

    right? I'm search for a good quality yet not expensive antenna which I

    can use with ST25RU3993 in order to achieve a reading distance of,

    let's say, at least 2 meters.

    Could someone point me one (or two)?

    Thanks!

    2019-11-19 12:38 GMT-03:00, ST Community:

    Visitor II
    December 5, 2019

    Hello jcbrtl,

    the kit comes with a near field antenna which allows you to read tags in the centimeter range only.

    For a start check:

    • Times7
    • Poynting
    • Laird
    • MTI Wireless Edge Ltd.
    • etc...

    For sure there a many more providers for good quality antennas!

    Cheers,

    B