ISO 14443 - Timing and AN6065
Hello to the support community,
i'm currently working on some custom coils used with the ST25R3916. I've studied the ISO/IEC 14443-2 for quite a while and recently had a look into the AppNote AN6065 from you guys.
There is quite some confusion on the topic stated in the AN around Figure 15.
First of: the minimum timing values stated in Table 3 are somewhat different from the ones in the actual ISO norm. That is not really the point of my question, but i just wanted you to know.
The real question arises from the following fact:
In the AN the Q factor of the coil is calcaulated to be Q<= 13.56 MHz * 3µs = 41. (The very bottom line on Page 18).
The 3µs represents the time that the unloaded coil would need to rise/ fall to the min/max amplitiude. So far so good.
Looking at this timing diagram:

I would expect that those 3µs would represent t3 or t1-t2 as those are the rise and fall times of the symbol. Looking in the table:
* t3 = 16/fc = 1.18µs
* t1-t2 = 2.98µs - steady_state_time
Obviously, t1 was used as the T for the T=1/B and thus the Q related calculation, which in my opinion does not make any sense as it is at least three times bigger, then the actual required rise/ fall times (t3, t1-t2).
Could you somehow explain why you only care about the circuit being damped to 5% at the very end of t1 rather then t1-t2?
Thank you and kind regards,
Tony