Solved
Linux driver for the CR95HF-based board
Posted on August 22, 2013 at 09:03
Hello, I am trying to make my m24lr discovery board work under Linux.
I've seen that ST provides a DLL to communicate with the green board under windows, but I'd like to use it under Linux. As far as I've seen, it is a HID device, but even by reading the source codice for its microcontroller, I've been only able to understand that the firmware forwards the commands to the CR95HF, but I was not able to understand the format of the commands. Do you have a working code to use that board under linux? Or do you have a bit more documentation, so that I can try to use the board with libusb? Thank you Ottavio #cr95hf #linux-driver-cr95hf #linux #linux-driver-cr95hf