M24LR-DISCOVERY question
Hi
I need to store a single file on the board from a PC (with ST application via USB) then I need to be able to read the file back to the PC (with ST application via USB). In addition, I need to be able to transfer the same file (via NFC) to any reader (i.e. smart phone)
I have only the ''RF transceiver board'' that is connected to the PC with USB.
I downloaded the demo application for it (stsw-m24lr011) but I can't make it communicate with the board via USB. Is there a way to store file on this board at all and if so, hot to accomplish this task?
Thanks a lot.
#nfc