M24LR04 energy harvesting shuts down with certain phones
We are evaluating the M24LR04 for a specific application where energy harvesting is required. We have configured the energy harvesting mode 3 to ensure that it will attempt to continue to harvest with low magnetic field strength. However, we regularly see the power supply shut down with certain phones. The Nexus 5, for example, will only harvest energy in a very narrow range between 5 and 8 mm distance and in a very narrow X, Y alignment window.
Is there anything we can do to help this? Why does the chip shut down energy harvesting at all? I would sooner let Vout sag than shut it down completely. Is there a different chip that we can use that will have better performance?