M24SR Capacitor frequency antenna tuning
Hello,
I would like to implement the M24SR02 in my design, with an NFC antenna.
The problem is that, in order to have a resonant frequency of 14.2MHz, the inductance of the NFC antenna needs to be around 5µH in order to resonate with the 25pF capacitance inside the M24SR02, but this value of inductance is difficult to reach with a small size antenna (<10mm).
Is it possible to add a capacitor between AC0 and AC1 pin, or two capacitors between the ACx pins and the ground, in order to make the capacitance higher, which will make the needed inductance of the antenna lower, and thus allows me to use a smaller antenna ?
Best regards,
Guillaume