M24SR64-Y Interrupt - GPO as INT configuration
Hello, everyone,
I have a problem with setting the GPO of M24SR64-Y as an INTERRUPT. The micro needs to come out of Sleep condition through an Interrupt sent from smartphone via RF, I saw that you have to set the GPO with 0x4X, but I don't know how to send this packet to set the GPO as INTERRUPT.
The bytes I send and receive are:
SYSTEM Select and UpdateBin with the GPO Field at 0x4X (can be seen in the attached figure).

(BLUE-SCL / RED-SDA / GREEN-GPO)
I receive as a response (R-APDU) from the module bytes 6A 82.
Could you please help me out? Do I also need to implement the Capability Container to set GPO as INT?
Also, the packet I send as SendInterrupt is as follows:
0x56, 0x02, 0xA2, 0xD6, 0x00, 0x1E, 0x00 + CRC (0xCA,0x7F)
wanted to know if this is correct as a structure or if something is missing
Thank you very much