Solved
My reader can read/write the M24LR04 but not M24LR16
Posted on August 20, 2013 at 11:49
Hello,
I'm using an RFID reader (Feig LRM1002) with 2 different version of the M24LRXX chip : - M24LR04E(ANT3-M24LR04E)
- M24LR16E(ANT1-M24LR16E and ANT2-M24LR16E)
A problem appear when I scan my tag :
When I send an ''Inventory'' command there are no problems, I can see both versions of the chip. The problem appear when I send a ''Read or Write Multiple Blocks'' command. With the M24LR16E I have an error message : ''No Transponder In Reader Field'' (it works well with the M24LR04E). I tried the ''Extended Adress Mode'' but it didn't change anything. Do you know what the problem could be ? For information I use the demo software provided by the reader manufacturer (Feig ISOStart). I took some screenshot : Thank you m24lr04e m24r04e 2-bytes m24lr16e devkit-m24lr-a m24lr-read-write-problem m24lr16e m24lr04e high-density