Skip to main content
Graduate II
November 3, 2023
Solved

NFC reader ST25R3916B EXT_LM pin

  • November 3, 2023
  • 1 reply
  • 897 views

Hi,
My application used ST25R3916B for transmit power for the card only.

1. Is it possible to leave the EXT_LM pin unused or exclude external load modulation from my application?
2. Can I use the testing point only on the pin EXT_LM pin?
Best,
Dalik LIM

 

    This topic has been closed for replies.
    Best answer by Ulysses HERNIOSUS

    Hi Dalik,

     

    not sure I completely understand: Using EXT_LM is a possibility in the chip. Technically it can work without. Foreseeing a testpoint is always a good idea.

     

    Regards, Ulysses

    1 reply

    Technical Moderator
    November 6, 2023

    Hi Dalik,

     

    not sure I completely understand: Using EXT_LM is a possibility in the chip. Technically it can work without. Foreseeing a testpoint is always a good idea.

     

    Regards, Ulysses