NFC Reader ST25R95
1. NFC ST25R95 Can I process if I don't use the MCU to control?
2. Can I boot up voltage to 10V for pin TX1 and TX2 for differential pair?
Best,
Dalik
1. NFC ST25R95 Can I process if I don't use the MCU to control?
2. Can I boot up voltage to 10V for pin TX1 and TX2 for differential pair?
Best,
Dalik
Hi,
I would recommend to use STM32CubeMX that will help you to define your clock tree for your MCU.
The STM32F030K6T6 is having a LQFP32 package where the OSC32-IN and OSC32-OUT pins are not present (thus it is not possible to use a Low Speed External 32.768 kHz crystal).
Depending on your application needs, you can clock your system either from the High Speed Internal (HSI) 8 MHz RC clock or from an High Speed External (HSE) 4-32 crystal (providing a better clock accuracy but of course with an impact on your BOM). See RM0360 Reference Manual §7 for the description of the various clock.
Rgds
BT
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.